Select a project file - error messages
If error messages display when selecting a
Logix Designer
, use this table to troubleshoot the issue.Error Message | Action to Take |
|---|---|
The specified Logix Designer project file was not found. | The file may have been renamed, moved, or deleted after it was selected in the Select Project File dialog box.In Windows Explorer, navigate to the file selected in the Select Project File dialog box, and verify that it still exists with the same name in the selected location. |
No revision of Logix Designer is installed. | Logix Designer is not installed on the same computer as FactoryTalk Batch Equipment Editor .Install Logix Designer revision 16.0 or higher on the same computer as FactoryTalk Batch Equipment Editor . |
The revision of Logix Designer required to open the project is not installed. | The installed revision of Logix Designer does not support PhaseManager functionality.Upgrade the current installation of Logix Designer to revision 16.0 or higher. |
The Logix Designer project file must be converted. The revision is too old. | The revision of the selected Logix Designer project file is lower than revision 16.0.Open the selected project file in Logix Designer revision 16.0 or higher to convert the file to this revision. |
The specified file is not a valid Logix Designer project file. The file format is not recognized or has been corrupted. | Try to open the selected project file in Logix Designer . If it does not open, the file format has been corrupted. |
The Logix Designer project file is read-only and cannot be opened. | Disable the Read-Only Attribute for the selected project file. In Windows Explorer, navigate to the selected file in the Select Project File dialog box. Open the Properties dialog box for the file and verify that the Read-Only Attribute is not selected. |
The Logix Designer project file revision does not support phases. Use revision 16.0 or greater. | The installed revision of Logix Designer and the selected project file is lower than revision 16.0. Upgrade the revision of Logix Designer to 16.0 or higher. Open the selected project file in Logix Designer to convert the file to the upgraded revision. |
Provide Feedback