Custom attributes

Custom attributes are user-defined properties of materials, lots or containers. Custom attributes can be accessed in addition to the standard attributes. Each property that is added in the
FactoryTalk Batch
Material Manager
material database has a controller ID, which begins at 1000 and increments by 10. Several types of data are made available for each attribute, which are indexes.
The attribute ID of the custom attribute calculates from the controller ID plus the index.
FTB_PCD Programmers Custom Index
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal