UnitIDOperations
The
UnitIDOperations
item returns a list of the equipment operation sequences within the unit specified by the unit ID.This table shows the input and output formats for this item.
Input Format | Request: UnitIDOperations | ||
UnitID | is | An ASCII - integer representing the | |
Output Format | The UnitIDOperations item returns in this format: | ||
<OperationsList> | is | <Operation> \crlf | <Operation> \crlf <OperationList> | |
<Operation> | is | <OpSeqID> \t <OpSeqName> \t <MaxOwners> \t <OperationType> \t <XCord> \t <YCord> \t <BitMapIndex> | |
where <Operation> is: | |||
Field Name | Format | Description | |
<OpSeqID> | ASCII - Integer | Equipment ID of the equipment operation sequence. | |
<OpSeqName> | ASCII - String | Name of the equipment operation sequence configured in FactoryTalk Batch Equipment Editor. | |
<MaxOwners> | ASCII - Integer | Maximum number of owners. | |
<OperationType> | ASCII - Integer | This is an equipment operation sequence, so this field is not used. | |
<XCord> | ASCII - Integer | X coordinate for the bitmap in the Equipment View. | |
<YCord> | ASCII - Integer | Y coordinate for the bitmap in the Equipment View. | |
<BitMapIndex> | ASCII - Integer | Location of bitmap in the List of Phase Bitmap items. This field is not used. | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(55Operations) could return:68 \t MAKE_CHOCOLATE_CUSTARD \t 1 \t 0 \t 95 \t 88 \t 0 \crlf 70 \t MAKE_VANILLA_CUSTARD \t 2 \t 0 \t 362 \t 89 \t 0 \crlf |
Provide Feedback