Order
The
ORDER
execute reorders the requester’s list for a resource.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[ORDER( Item,UserID,ResourceID,OwnerID,NextOwnerID,
Position )] | |
where: | Item | Item name as specified by the client. |
UserID | User identification entered into the event journal associated with this event. | |
ResourceID | Resource’s Equipment ID whose requester’s list is to be reordered. | |
OwnerID | Resource’s unique ID to be moved in the requester’s list. | |
NextOwnerID | Resource’s unique ID, in the position within the requester’s list, which the OwnerID is requesting. If Position is RELATIVE, the OwnerID resource will be positioned prior to the NextOwnerID resource. | |
Position | Position within the requester’s list in which the resource should be placed:
| |
Action | A successful ORDER execute results in a change to the requester’s list for the ResourceID. | |
Return Format | The item populates with this data: SUCCESS: | FAIL: <message> | FAILED | |
The following table shows an example of the return on this execute.
Example: | An execute string: ORDER(Item,UserID,12,22,1,RELATIVE) |
Provide Feedback