Place the Batch Phase Execution control on a form
Use
Visual Basic
to place the Batch Phase Execution
control on a form.To place the Batch Phase Execution control on a form
:- Select theBatch Phase Executioncontrol in theVisual Basictoolbox.
- Position the cursor on the form where you want the control.
- Click and drag to draw the outline of the control on the form.
- Release the outline to place the newBatch Phase Executioncontrol at the location specified. The PC-based phase can now be programmed.
Provide Feedback