Phase commands
The for additional information on legal state
transitions.)
FactoryTalk Batch
Phase Simulator allows you to change the state of a phase. An active phase can be
commanded to COMPLETE without gaining phase ownership. All other state change commands
require the phase be under external control. The Start/Stop
, Abort/Reset
and
Hold/Restart
buttons are modal, in that the command issued is determined based on
the phase’s active state at the time the button is clicked. Only legal state change commands
are executed. For example, if a phase is RUNNING and the Start/Stop
button is
clicked, the STOP command is issued. START is not a legal command to a phase in the RUNNING
state. (Refer to the FactoryTalk Batch
PCD Programmer Technical Reference Guide This table shows the phase’s transition when the state change command is received, along with the associated state value (
##
).COMMAND | INITIAL STATE | FINAL STATE |
|---|---|---|
COMPLETE | COMPLETE (70) | |
START | RUNNING (50) | |
STOP | STOPPING (30) | STOPPED (80) |
ABORT | ABORTING (10) | ABORTED (90) |
RESET | IDLE (100) | |
HOLD | HOLDING (20) | HELD (60) |
RESTART | RESTARTING (40) | RUNNING (50) |
Provide Feedback