Batches
Use Batches to create, view, and command a control recipe, observe the execution of a single recipe, and bind units for class-based recipes. Once a control recipe is created, it remains in the
Batches
list until it is removed or until the FactoryTalk Batch
Server is restarted with a cold boot. A graphical representation of a running batch and its associated data is displayed. Try it: Create a control recipe
- SelectBatches.
- SelectAdd
.
- Select a master recipe.
- Enter a unique batch ID.TIP: The Batch ID box accepts non-unique IDs. When duplicate batch IDs are used, it is difficult to associate prompts with the correct batch when viewed in Prompts.
- (optional) Perform any of these:
- To run a batch at a percentage other than 100%, in theBatchScalebox, enter the percentage.
- To change the description of the batch, in theDescriptionbox, enter a new description.
- If the recipe contains a material class-based phase, select the material to use in this particular batch.
- To assign or change a formula value, enter new values inFormula Values.
- Select the equipment for the control recipe in theUnit Bindingsarea. TheUnit Bindingarea appears after selecting all required parameters. By default, the equipment is not selected. The user must configure the equipment manually. A unit binding error appears if a configuration error occurs. For detailed information, SelectSelect for details.
- SelectCreate
to add the control recipe to the
Batcheslist.
Provide Feedback