FactoryTalk Security for the Batch Clients
Security settings are shared among
FactoryTalk
enabled products across a network or on the same computer using FactoryTalk
Security in FactoryTalk Batch View
, HMI Controls, FactoryTalk Batch Equipment Editor
, and FactoryTalk Batch Recipe Editor
. FactoryTalk
Directory is the infrastructure which contains the policies defined for products and
resources. FactoryTalk Batch
product policies are created in both the Local Directory and the Network Directory when
the FactoryTalk
Services Platform is installed. The FactoryTalk Batch
product polices are used to restrict access to the FactoryTalk Batch
Client components and their features. For a complete list of FactoryTalk Batch
secured resources and their default product policy settings, see FactoryTalk Batch
default policy settings.The following information is specific to configuring .
FactoryTalk
Security for the FactoryTalk Batch
Clients. For information on securing your FactoryTalk
system as a whole, see FactoryTalk
HelpTo open
FactoryTalk
Help, click Start > Rockwell Software >
. FactoryTalk
HelpThe
FactoryTalk
Services Platform installation process:- Creates aWhen the install process finishes, both directories are fully configured and ready for use.FactoryTalkLocal Directory and aFactoryTalkNetwork Directory on the computer.TIP:Security settings in the Network Directory are completely separate from the security settings in the Local Directory. For example, changes made to the security settings in the Network Directory do not change security settings in the Local Directory.
- Allows any Windows Administrator user account to log on to either directory.The installation process automatically adds the local Windows Administrators group to theFactoryTalkAdministrators group in eachFactoryTalk Directory.
- Allows any authenticated Windows user to log on to theThe installation process automatically adds all members of the local Windows Authenticated Users group to theFactoryTalkLocal Directory.FactoryTalkLocal Directory.
- Allows all new user accounts full access permissions.The installation process automatically sets system policies to allow all new user accounts added to either directory full access to that directory by default.
Provide Feedback