Local Path Name line format example
Line Format (Local Path Name)
C:\path_to_journal_file \t REMOVED{CR/LF}
Example
C:\Program Files\Rockwell Software\Batch\SAMPLEDEMO1\journals\123.evt \t REMOVED{CR/LF}
C:\Program Files\Rockwell Software\Batch\SAMPLEDEMO1\journals\124.evt \t REMOVED{CR/LF}
C:\Program Files\Rockwell Software\Batch\SAMPLEDEMO1\journals\125.evt{CR/LF}
Provide Feedback