Archque.txt file
The archive queue file,
ArchQue.txt
, contains a list of electronic batch record
files. The line format within the list contains the path and file name of the batch record
file. The path name can use either UNC names or local path names, depending on the
definition of the journal project directory in the FactoryTalk Batch
Equipment Editor Server Options
dialog box. 
If a batch is removed from the batch list, a tab character (\t) and the word REMOVED follows the file name. Each electronic batch record file is listed in a single record delimited with Carriage Return / Line Feed (CR/LF).
TIP:
Keep the
ArchQue.txt
file locked while it is open and keep it open for only a few
seconds. When the queue file is open for more than a few seconds, the FactoryTalk Batch
Server cannot add entries to the queue as other control recipes are created.
IMPORTANT:
The
ArchiverEnabled=Never
setting in the BatchArc.ini
file causes the Archiver queue file to not be written. To write to this queue file, use a setting other than Never
, and manually maintain the size of the archive queue file.Provide Feedback