Acquire
The
ACQUIRE
execute acquires a resource for the operator.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[ACQUIRE( Item,UserID,OwnerID,ResourceID )] | |
where: | Item | Item name as specified by the client. |
UserID | User identification associated with this event. | |
OwnerID | Identification of the operator. | |
ResourceID | Equipment ID of the resource to be acquired. Configure this value in FactoryTalk Batch Equipment Editor . | |
Action | A successful ACQUIRE execute places operator into the requester’s specified resource list. When the resource determines that the operator can become an owner, then operator moves into the owner’s resource list. | |
Return Format | The item populates with this data: SUCCESS: | FAIL: <message> | FAILED | |
The following table shows an example of the return on this execute.
Example: | An execute string: [ACQUIRE(Item,Station5\Operator,0,119)] |
Provide Feedback