ResourceIDInfo
The
ResourceIDInfo
item returns the resource name denoted by the resource ID.This table shows the input and output formats for this item.
Input Format | Request: ResourceIDInfo | ||
ResourceID | is | ASCII - String, the | |
Output Format | The ResourceIDInfo item returns in this format: | ||
<ResourceInfo> | is | <ResourceInfo> | |
where: | |||
Field Name | Format | Description | |
<ResourceInfo> | ASCII - String | The name of the resource prefaced with the type of resource: Procedure (for Operator)
Process Cell
Unit
Phase
Resource | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(68Info) could return:Phase NP_ADDDAIRY_M1 |
Provide Feedback