DDEClientCount

The
DDEClientCount
item returns the number of DDE clients connected to the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
DDEClientCount
Output Format
The DDEClientCount item returns in this format:
<DDECount>
Field Name
Format
Description
<DDECount>
ASCII - String
Number of DDE clients connected to the
FactoryTalk Batch
Server.
This table shows an example of the return on this request.
TIP:
A request on the
object.GetItem(DDEClientCount)
could return:
1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal