Upload the reports configured for upload on transfer of control

Configure the PXRQ instruction in
Logix Designer
to upload values for reports configured for upload on transfer of control:
External Request
Data Value Array Element
Value
Upload Output Parameters Subset
DINT[0]
2
Assign reports to this subset in
FactoryTalk Batch Equipment Editor
.
If the phase associated with the report parameters enabled control strategies, only those report parameters belonging to
both
the enabled control strategy and the specified subset will be included in the upload.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal