Generate an electronic signature request

During batch execution, phase logic can issue a request to the
FactoryTalk Batch
Server to generate a Signature Request. Each Signature Template is assigned a unique ID, which is a positive integer. Requests to generate a Signature specify the desired Signature Template ID. Configure the PXRQ instruction in
Logix Designer
to generate an electronic signature request:
Generate E Signature
DINT[0]
signature template ID
DINT[1]
Defines if signature is able to be canceled:
0 = No
non-zero = Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal