Illegal characters encountered in writing instruction file

Because the contents of instruction files are included (that is, putting them into a CDATA section), it is possible that the particular character sequence ]]>, which is illegal in CDATA sections, might be encountered.
If this character sequence is encountered, this error message displays and the export does not occur.
FTB_EE_XML_export_IllegalCharacter_B12
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal