PhaseIDState
The
PhaseIDState
item returns the current state for a phase or an equipment operation sequence. This table shows the input and output formats for this item.
Input Format | Request: PhaseIDState | ||
PhaseID | is | Unique equipment ID corresponding to the phase or equipment operation sequence. | |
Output Format | The PhaseIDState item returns in this format: <StateText> | ||
Field Name | Format | Description | |
<StateText> | ASCII - String | Value corresponding to the state register’s value in the process-connected device. If this value does not correspond to any defined batch state, displays ??? . | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(68State) could return:IDLE |
Provide Feedback