HyperlinkLabels
The
HyperlinkLabels
item returns a tab-delimited list of hyperlink labels for each equipment type: process cells, units, equipment phases, and shared resources. Each equipment type can contain up to five hyperlink labels.This table shows the input and output formats for this item.
Input Format | Request: HyperlinkLabels | ||
Output Format | The HyperlinkLabels item returns in this format: <PCellLabels> \crlf <UnitLabels> \crlf <PhaseLabels> \crlf <ShResrcLabels> | ||
where: | |||
<PCellLabels> | is | <PCL1> \t <PCL2> \t <PCL3> \t <PCL4> \t <PCL5> | |
<UnitLabels> | is | <UL1> \t <UL2> \t <UL3> \t <UL4> \t <UL5> | |
<PhaseLabels> | is | <PL1> \t <PL2> \t <PL3> \t <PL4> \t <PL5> | |
<ShResrcLabels> | is | <SRL1> \t <SRL2> \t <SRL3> \t <SRL4> \t <SRL5> | |
where: | |||
Field Name | Format | Description | |
<PCL#> | ASCII – String | Where # is an integer from 1 through 5. Hyperlink label for a process cell. | |
<UL#> | ASCII – String | Where # is an integer from 1 through 5. Hyperlink label for a unit. | |
<PL#> | ASCII – String | Where # is an integer from 1 through 5. Hyperlink label for a phase. | |
<SRL#> | ASCII – String | Where # is an integer from 1 through 5. Hyperlink label for a shared resource. | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(HyperlinkLabels) could return:Hyperlink Label 1 English Process Cell \t Hyperlink Label 2 English Process Cell \t Hyperlink Label 3 English Process Cell \t Hyperlink Label 4 English Process Cell \t Hyperlink Label 5 English Process Cell \crlf Hyperlink Label 1 English Unit \t Hyperlink Label 2 English Unit \t Hyperlink Label 3 English Unit \t Hyperlink Label 4 English Unit \t Hyperlink Label 5 English Unit \crlf Hyperlink Label 1 English Phase \t Hyperlink Label 2 English Phase \t Hyperlink Label 3 English Phase \t Hyperlink Label 4 English Phase \t Hyperlink Label 5 English Phase \crlf Hyperlink Label 1 English Resource String \t Hyperlink Label 2 English Resource String \t Hyperlink Label 3 English Resource String \t Hyperlink Label 4 English Resource String \t Hyperlink Label 5 English Resource String \crlf |
Provide Feedback