Material Usage Report
Material Manager
automatically creates these parameters:Formula Parameter: | material |
Report Parameter: | actual_amount |
Without
Material Manager
, define these Formula and Report parameter names:Formula Parameter: | material_xx (where xx is user defined) |
Report Parameter: | actual_xx (where xx is user defined) |
Add phase example
:Formula Parameter: | material_oil |
Report Parameter: | actual_oil |
-or-
Add phase example
:Formula Parameter: | material_oil |
Formula Parameter: | material_water |
Report Parameter: | actual_oil |
Report Parameter: | actual_water |
Provide Feedback