Special considerations – naming conventions
Batch reporting uses naming conventions in the
FactoryTalk Batch
Area Model when Material Manager
is not used.Standard
Material Manager
supplies data for these reports so these naming conventions are not needed.Provide Feedback