Setpoint vs. Actual
Material Manager
automatically creates these parameters:Formula Parameter: | amount |
Report Parameter: | actual_amount |
Without
Material Manager
, define these Formula and Report parameter names:Formula Parameter: | setpoint_xx (where xx is user defined) |
Report Parameter: | target_xx (where xx is user defined) |
Report Parameter: | actual_xx (where xx is user defined) |
Report Parameter: | in_tolerance_xx (where xx is user defined) |
Report Parameter: | target_xx is optional |
Report Parameter: | n_tolerance_xx is optional |
Add phase example
:Formula Parameter: | setpoint_oi |
Report Parameter: | actual_oil |
Report Parameter: | in_tolerance_oil |
Add phase example
:Formula Parameter: | setpoint_oil |
Report Parameter: | target_oil |
Report Parameter: | actual_oil |
Report Parameter: | in_tolerance_oil |
Provide Feedback