Forward/Backward Track and Trace Report
Material Manager
automatically creates these parameters:Formula Parameter: | lot |
Report Parameter: | actual_amount |
Without
Material Manager
, define these Formula and Report parameter names:Report Parameter: | lot_xx_yy (where xx is user defined and yy represents an incremental lot #) |
Report Parameter: | actual_lot_xx_yy (where xx is user defined and yy [optional] represents an incremental lot ) |
Single lot with single actual. Without yy value. | |
Add phase example
:Report Parameter: | lot_oil |
Report Parameter: | actual_lot_oil |
Single lot with single actual. With yy value. | |
Add phase example
:Report Parameter: | lot_oil_01 |
Report Parameter: | actual_lot_oil_01 |
Multiple lots with multiple actuals. | |
Add phase example
:Report Parameter: | lot_oil_01 |
Report Parameter: | lot_oil_02 |
Report Parameter: | actual_lot_oil_01 |
Report Parameter: | actual_lot_oil_02 |
Provide Feedback