FactoryTalk Batch Database Manager

The
FactoryTalk Batch Database Manager
is designed to provide assistance in performing backup, delete, and restore operations on the
FactoryTalk Batch
Archiver (BatchHistoryEx) database, based on date. When the
FactoryTalk Batch Database Manager
is launched, choose to backup and delete database records or restore database information from a backup.
Backups are in the form of a Microsoft SQL Server backup (
.bak
) file or to a remote Microsoft SQL Server database. The
.bak
option is used to restore the original data to a database with a new name. The remote database option creates an identical database on another machine. The database has an identical schema to the
FactoryTalk
Batch Archiver database. All records deleted from the
FactoryTalk Batch
Archiver database are first backed up to the database or to a
.bak
file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal