Restore database information from a backup

The Restore option creates a new database of
FactoryTalk Batch
records from a backup previously generated by the
FactoryTalk Batch Database Manager
. This does not restore into the Batch Archiver database.
To restore database information from a backup:
  1. In
    Restore Settings
    , enter the backup file and destination data source name.
  2. Enter a name for the restore database.
  3. Select
    Restore
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal