Grace periods in FactoryTalk Batch Server

When the
FactoryTalk Batch
Server starts, it performs a license check. If a valid activation is found, a successful license check is returned to the server. As a result of the license check, the server determines which applications have a license.
If its normal license check process fails, the server requests grace period activation from
FactoryTalk Batch
Activation. The manner in which the grace period activation is requested depends on the area model and why the license check process failed. The server will log the request for, and receipt of, the grace period license.
When grace period activation is requested for multiple activations by one process, the grace period is ended and the timer reset when any of the multiple activations can be successfully obtained.
Every four hours the
FactoryTalk
Activation software attempts to check out each activation requested as a grace period activation by the
FactoryTalk Batch
Server. If any one of these activations is successfully checked out, the grace period for the server ends.
TIP:
If the
FactoryTalk Batch
Server is started in the Demo mode, an exception is made to the license and unit checks. Even if no licenses are found, the server will run for two hours and then shut down.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal