Upload the reports configured for upload on terminal state

Configure the PXRQ instruction in
Logix Designer
to upload values for reports configured for upload on terminal state:
External Request
Data Value Array Element
Value
Upload Output Parameters Subset
DINT[0]
1
Reports are assigned to this subset in
FactoryTalk Batch Equipment Editor
.
If the phase associated with the reports enabled control strategies, only those reports belonging to
both
the enabled control strategy and the Upload on Terminal State subset will be included in the upload.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal