UnitIDBatchID
The
UnitIDBatchID
item lists the operator-entered batch ID for the batch to which the unit belongs.This table shows the input and output formats for this item.
Input Format | Request: UnitIDBatchID | ||
UnitID | is | ASCII - Integer, the | |
Output Format | The UnitIDBatchID item returns in this format: | ||
<BatchID> | is | ASCII - String (user defined) | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(55BatchID) returns:Batch_100 |
Provide Feedback