EventDataFiles
The
EventDataFiles
item returns the list of event data files in the system.This table shows the input and output formats for this item.
Input Format | Request: EventDataFiles | ||
Output Format | The EventDataFiles item returns in this format: | ||
<EvtDataFiles> | is | <NullList> | <EvtFileList> | |
<EvtFileList> | is | <EventFile> | <EventFile> <EvtFileList> | |
<EventFile> | is | <BatchID> \t <CreateID> \t <Description> \t <FilePath> \t <StartTime> \t <RecipeName> \crlf | |
where <EventFile> is: | |||
Field Name | Format | Description | |
<BatchID> | ASCII - String | Operator-entered batch ID number. | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server. | |
<Description> | ASCII - String | Procedure description from FactoryTalk Batch Recipe Editor . | |
<FilePath> | ASCII - String | Complete file name and event file path as defined in the batchsvr.ini file under [EventManager] section, EventDirectoryPath item. | |
<StartTime> | ASCII - String | Time at which the batch started. May be a blank space character if the batch has not yet started. | |
<RecipeName> | ASCII - String | Recipe file name. | |
This table shows an example of the return on this request.
TIP:
A request on
object
.
GetItem(EventDataFiles)
could return:BATCH_98 \t 15 \t French Vanilla Premium - class based \t \\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH
\SAMPLEAPP\JOURNALS\15.evt \t \t CLS_FRENCHVANILLA \crlf
BATCH_99 \t 16 \t French Vanilla Premium - class based \t \\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH
\SAMPLEAPP\JOURNALS\16.evt \t \t CLS_FRENCHVANILLA \crlf
BATCH_100 \t 17 \t French Vanilla Premium - class based/material based \t \\STATION5\PROGRAM FILES\ROCKWELL SOFTWARE\BATCH\SAMPLEAPP\JOURNALS\17.evt \t 2022.02.24 16:20:54 \t MCLS_FRENCHVANILLA \crlf
Provide Feedback