Create a new project
Use Microsoft
Visual C++
to add the Batch Phase Execution
control to a project.To create a new project
:- Start the MFC AppWizard executable.
- Select theDialog Basedoption.
- Ensure that support for ActiveX Controls is selected.
- Use MFC as a shared DLL.
Provide Feedback