Program the PC-based phase

The PC-based phase requires specific methods and events to function properly. These methods and events are predefined in the
Batch Phase Execution
control, and must be programmed for the specific PC-based phase being created. The following describes each of the required methods, along with example code for the
OnRestart
event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal