Generic Multiple Ingredient Addition Phase with multiple lots per material

This is an example of Generic Multiple Ingredient Addition Phase with multiple lots per material:
Additional Phase:
Add_Hand Adds
Formula Parameter:
Material_01
Formula Parameter:
Material_02
Formula Parameter:
Setpoint_01
Formula Parameter:
Setpoint_02
Report Parameter:
Lot_01_01
Report Parameter:
Lot_01_02
Report Parameter:
Lot_02_01
Report Parameter:
Lot_02_02
Report Parameter:
Actual_Lot_01_01
Report Parameter:
Actual_Lot_01_02
Report Parameter:
Actual_Lot_02_01
Report Parameter:
Actual_Lot_02_02
Report Parameter:
Target_01
Report Parameter:
Target_02
Report Parameter:
Actual_01
Report Parameter:
Actual_02
Report Parameter:
In_Tolerance_01
Report Parameter:
In_Tolerance_02
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal