Sequential Function Chart
In the
FactoryTalk Batch Recipe Editor
, create a sequential function chart (SFC) to represent the recipe logic flow. SFC provides a more flexible alternative to creating recipes. SFC methodologies define each recipe procedure and equipment. Benefits of SFC:
- Unambiguous representation of logic.
- Support for all important logic structures: decisions, loops, and parallelism.
- Standardized in IEC 61131-3 specification.
Provide Feedback