OPCClientCount

The OPCClientCount item returns the number of OPC clients connected to the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
OPCClientCount
Output Format
The OPCClientCount item returns in this format:
<OPCCount>
where:
Field Name
Format
Description
<OPCCount>
ASCII – String
Number of OPC clients connected to the
FactoryTalk Batch
Server.
This table shows an example of the return on this request.
Example:
A request on
object
.
GetItem(OPCClientCount)
could return:
2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal