DecimalSeparator

The
DecimalSeparator
item returns the decimal symbol used by the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
DecimalSeparator
Output Format
The DecimalSeparator item returns in this format:
<Character>
Field Name
Format
Description
<Character>
ASCII – String
Decimal character for the language-specific operating system.
This table shows an example of the return on this request.
Example:
A request on
object.GetItem(DecimalSeparator)
could return:
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal