Completion of messages
A and a
Send Message Wait
Receive Message Wait
request pair is complete only if the message IDs for each of the calls are identical. This prevents messages from being routed to the improper request. Additionally, the Send Message Wait
call must specify the number of receives confirmed as a parameter. This number allows for synchronization groups with more than two members.Provide Feedback