Download sufficient material data

Configure the PXRQ instruction in
Logix Designer
to download information regarding the availability of sufficient material, across all the valid binding candidates, to complete the addition before starting the material addition for the step.
External Request
Data Value Array Element
Value
Download Sufficient Material
DINT[0]
Phase parameter tag address of priority to be assigned.
DINT[1]
DINT[2]
The
FactoryTalk Batch
Server downloads one of these values about sufficient material for step:
Value
Description
0
Insufficient material was available across the valid binding candidates at the time the binding query was performed.
1
Sufficient material was available across the valid binding candidates at the time the binding query was performed.
TIP:
When the
FactoryTalk Batch
Server runs without the Material Server, it returns a ‘0’ or ‘1’ depending on when communication is lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal