Upload container attributes
Configure the PXRQ request in
Logix Designer
to upload one attribute of a container from a specified report ID. The attribute identified by the attribute ID uploads from the specified report ID into the database if security and write-protections allow. Only one value may be uploaded at a time.External Request | Data Value Array Element | Value |
Upload Material Manager Database Data | DINT[0] | 8 |
DINT[1] | Report ID that container data uploads from. | |
DINT[2] | Container Controller ID | |
DINT[3] | Attribute ID |
TIP:
The data type in the controller must match the data type of the report ID specified in the data value array element DINT[1].
Provide Feedback