Modify FactoryTalk Batch Equipment Editor configuration options

Modify the configuration options in product policies created in the
FactoryTalk
Local Directory for the editors.
The following example is specific to
FactoryTalk Batch Equipment Editor
.
FactoryTalk Batch Recipe Editor
configuration options are configured similarly.
:
  1. Open the
    FactoryTalk
    Administration Console and then log on to the
    FactoryTalk
    Local Directory
    .
  2. Expand
    System > Policies > Product Policies > Batch > Equipment Editor > Configuration
    .
  3. Right-click
    Options
    and then select
    Properties
    .
  4. From the
    Options Properties
    dialog box, configure the policy settings and then select
    OK
    .
    TIP:
    Restart all
    FactoryTalk Batch
    components to update changes made in the
    FactoryTalk Directory
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal