Phase execute command
The
PHASE
execute commands a phase or an equipment operation sequence to a specified state.The operator must own the phase or equipment operation sequence in order to change it.
The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[PHASE( Item,UserID,EquipmentID,Cmd,BatchID,Unit )] | |
where: | Item | Item name as specified by the client. |
UserID | User identification entered into the event journal associated with this event. | |
EquipmentID | Unique equipment ID for the phase or equipment operation sequence. | |
Cmd | Command for the phase or equipment operation sequence. Valid commands are:
START, STOP, RESET, RESUME, HOLD, RESTART, PAUSE, ABORT, DOWNLOAD, DISCONNECT, AUTO-MODE, SEMIAUTO-MODE, CLEAR_ FAILURES | |
BatchID | Identifier for the batch that is required for journals associated with this phase or equipment operation sequence. | |
Unit | Name of the unit to use with the phase or equipment operation sequence. | |
Action | A successful PHASE execute results in the specified command either being queued pending a signature confirmation, or being issued to the specified phase or equipment operation sequence. If the command is valid and a batch does not already exist for manual control of the phase or equipment operation sequence, then a batch is created using the specified BatchID and Unit .A failure message is generated when the following occurs:
| |
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | FAILED | |
where: | ||
Field | Format | Description |
<ActionID> | ASCII – Integer | Identifier associated with the signature(s) generated in response to the execute. |
<message> | ASCII - String | Error message appropriately formatted for operator display. |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: PHASE(Item,Station2/View,29,START,MAKESTUFF,BIGMIXER) Could return: SUCCESS:997 |
Provide Feedback