Download container attributes

Configure the PXRQ instruction in
Logix Designer
to download one attribute of a container to a specified parameter ID. The attribute identified by the attribute ID downloads into the tag specified. Only one value may be downloaded at a time.
Download
Material Manager
Database Data
DINT[0]
3
DINT[1]
Parameter ID container data downloads to.
DINT[2]
Container Controller ID
DINT[3]
Attribute ID
TIP:
The data type in the controller must match the data type of the parameter or report ID specified in the data value array element DINT[1].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal