BLCreateID_x
BLCreateID_x returns the CreateID for the batch in the batch list.
x
thThis table shows the input and output formats for this item.
Input Format | Request: BLCreateID_ <RowNumber> | ||
<RowNumber> | is | ASCII - Integer An array index. When an unacknowledged prompt generates, it adds to an array. If the unacknowledged prompts list is not sorted, then x is the row number of the unacknowledged prompt appearing in the unacknowledged prompts list. | |
The BLCreateID_x item requires the Batchsvr.ini file to contain this setting in the [CLIENT MGR DDE] section:MaxBatchTableLength = n where n is the maximum number of batches accessible to this Item (the maximum number of entries in the array). If the number of batches in the batch list is larger than n , then this item will only access the first n batches in a non-sorted batch list. When a batch with an index of less than n is removed from the batch list, all subsequent batches will have their index decreased by one. The default value of MaxBatchTableLength is 0 (zero). | |||
Output Format | The BLCreateID_x item returns in this format: <CreateID> | ||
Field Name | Format | Description | |
<Create ID> | ASCII – Integer | Unique identifier assigned by the FactoryTalk Batch Server to the batch appearing on the x th | |
This table is an example of a typical batch list containing three batches with batch IDs BATCH_98, BATCH_99, and BATCH_100:
Create ID | Batch ID | Recipe | Desc | Start Time | State | Mode |
15 | BATCH_98 | Vanilla | Ice Cream 1 | 8/24/2017 1:22:02 pm | RUNNING | O_Auto |
16 | BATCH_99 | Chocolate | Ice Cream 2 | 8/24/2017 1:24:12 pm | RUNNING | S_Auto |
17 | BATCH_100 | Premium French Vanilla | Ice Cream 3 | 8/24/2017 1:32:30 pm | RUNNING | O_Auto |
This table shows an example of the return on this request.
TIP:
A request on
object.GetItem(BLCreateID_3)
would return the CreateID of the batch in the batch list’s third row: 17
Provide Feedback