Run FactoryTalk Event Archiver
When using End of Batch Archiving, the
FactoryTalk Batch
Server runs FactoryTalk Event Archiver
after a batch is removed from the batch list. When using Incremental Archiving, FactoryTalk Event Archiver
runs continuously during batch execution and archives batch data at user-defined time increments. The FactoryTalk Batch
Service Manager controls the Archiver Service. The Batch Service Manager must communicate with the Windows Service Manager of the selected computer to determine available services. A noticeable delay may exist while communications are established. If the Batch Service Manager cannot communicate with the Windows Services, an error message is displayed.
Before you begin
:- Ensure the computer whereFactoryTalk Event Archiveris installed has administrative privileges.
To run
:- SelectStart > Rockwell Software > Batch Service Manager.
- On thedialog box, chooseFactoryTalk BatchService ManagerSelect Computer.
- On theSelect Computerdialog box, select the name of the computer where the Archiver Service is installed, and then selectOK. TheSelect Computerdialog box closes.
- From theServicelist, select.FactoryTalk Event Archiver
- SelectStartto start theFactoryTalk Event ArchiverService and then selectClose.

Provide Feedback