Release resources

During batch execution, phase logic can issue a request to the
FactoryTalk Batch
FactoryTalk Batch
Server to release a resource. Each resource configured with
FactoryTalk Batch Equipment Editor
has an equipment ID, a positive integer. Requests to release a resource refer to the resource using the equipment ID. Only resources that were previously acquired with an
Acquire Resources
phase request can be released using the
Release Resources
phase request.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal