Release multiple resource values
Configure the PXRQ instruction in
Logix Designer
to release multiple resources:External Request | Data Value Array Element | Value |
Release Resources | DINT[0] | Equipment ID |
DINT[1] | Equipment ID | |
DINT[2] | Equipment ID |
Release up to 99 resources with this request. The
FactoryTalk Batch
Server releases the resources associated with the equipment IDs if this phase previously acquired the resources through an Acquire Resources
request.Provide Feedback