Add control events

Use the resource ID of the phase for each event to add control events.
To add control events
:
  1. Right-click the
    Batch Phase Execution
    control’s icon.
  2. Select the event.
  3. Double-click the event.
  4. Edit the member function name as desired and click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal