Set security on folders or files
Limit log file and event journal (.evt or .evtj) access to prevent data from being lost. Setting security on the folders or files is one suggested method. Set the security according to company requirements.
Use Notepad to open log files. If a log file is opened with a program other than Notepad,
the
FactoryTalk Batch
Server may not run due to an access error.
IMPORTANT:
FactoryTalk Batch
Server continues writing information to log files and event journals (.evt
or
.evtj
) even when they are open. If a file is opened and then saved, data that may
have been written to the event journal or log file while the file is open is lost.To set security on folders or files
:- InWindows Explorer, locate the folder or file.
- Right-click the folder or file, and then selectProperties.
- Select theSecuritytab, selectEdit, and then selectAdd.
- From theSelect Users, Computers, Service Accounts, or Groupsdialog box, selectAdvancedand then selectFind Now.
- Select a user or group from the Search results list, and then selectOK.
- Repeat for each user or group that requires access to the folder or file.NOTE:Be sure to add theFactoryTalk BatchServer user account and then configure the account withFull Controlpermissions.
- SelectOKto return to thePropertiesdialog box.
- From theGroup or user namelist, select a user or group, and then select the permissions in thePermissionsarea. Repeat for each user or group.
- SelectOK.
Provide Feedback