Batch View Errors
When running batches, you may occasionally encounter situations that are difficult to resolve. This section provides solutions to some of the problems you may encounter.
Issue | Solution |
|---|---|
The following error displays when running a batch:
Recipe SFC Requires Illegal Use of Dedicated Resources . As a result, the batch goes into a HELD state. | Parallel steps requesting the same equipment module cannot occur just after an AND Divergence.
|
A batch seems to be running, but it is not progressing as it should. No errors are generated. The status is RUNNING. | Parallel steps requesting the same equipment module cannot occur just before an AND Convergence.
|
A failure is generated and the batch is held because the Batch server selected an equipment phase under EXTERNAL control to bind to during batch execution. | Phases put into an external state can still be viewed as binding candidates by the FactoryTalk Batch Server. (The external state is a tag in the controller that prevents the Server from controlling the phase.) To remove a phase from being viewed as a binding candidate, you must take ownership of the phase. (For more information on the External attribute, see the PCD Programmer’s Guide. ) |
Provide Feedback