CreateIDScale
The
CreateIDScale
item returns the scale factor defined during batch creation.This table shows the input and output formats for this item.
Input Format | Request: CreateIDScale | ||
CreateID | is | ASCII – Integer, INTERNAL identifier assigned during batch creation. Obtain from the BatchList item. | |
Output Format | The CreateIDScale item returns in this format: <ScaleText> | ||
where: | |||
Field Name | Format | Description | |
<ScaleText> | ASCII – Integer | String representation of batch scale where 1 represents 100% and 0.5 would be 50%. | |
This table shows an example of the return on this request.
TIP:
A request on the
object.GetItem(3scale)
could return: 0.75
Provide Feedback