Available items
List of all supported items in the
FactoryTalk Batch
Server API:Item | Description |
|---|---|
Number of tags, phases, and equipment operation sequences on which verification failed. | |
List of all created batches. | |
Batch list count. | |
Returns the number of Parameter Expression Overrides currently in effect for each batch on the batch list. | |
Identifier for a batch. | |
Command mask for a batch. | |
Create identifier for a batch. | |
Description for a batch. | |
Highest priority failure message for a batch. | |
Mode for a batch. | |
Recipe for a batch. | |
Start time for a batch. | |
State for a batch. | |
Type for a batch. | |
Number of COM clients connected to the FactoryTalk Batch Server. | |
CPR version of the FactoryTalk Batch Server. | |
List of all steps in a recipe. | |
List of all steps in a recipe (allows displaying of override status of a parameter). | |
Most recent data for a batch. | |
Name of a batch data file. | |
Scale factor for a batch. | |
Information about all of the data servers defined for the equipment database. | |
Detailed description of each configured data server conversation and the status of each conversation. | |
Number of DDE clients connected to the FactoryTalk Batch Server. | |
Decimal symbol used by the FactoryTalk Batch Server. | |
List of the domain names available for authenticating users attempting signoffs on signature requests. | |
List of enumerations within a specified enumeration set. | |
Path and file name of the equipment model in use. | |
Date of the equipment model in use. | |
The number of times the equipment model in use has been updated. | |
Most recent severe message in the server’s log file. | |
List of event data fields in the system. | |
Current expression values for each term in the expression. | |
Current expression values for each term in a report expression. | |
Current expression value and all of its leaf node values for a given expression or unit association. | |
Tab-delimited list of hyperlink labels for each equipment type. | |
Count of all incomplete signature requests, excluding those generated by private interfaces. | |
Most recent information message in the server’s log file. | |
Number of items created by the FactoryTalk Batch Server that are exposed through DDE and COM. | |
Path to the journals directory. | |
List separator used by the FactoryTalk Batch Server, as read from Control Panel > Regional Options . | |
Locale identifier (language ID and code page) used by the FactoryTalk Batch Server, as read from the Control Panel . | |
Returns the path to the error log directory specified in the batchsvr.ini file at the time the FactoryTalk Batch Server was started. | |
List of all phases in the system. | |
Number of OPC clients connected to the FactoryTalk Batch Server. | |
Information about all of the equipment operation sequences in the system. | |
List of all the equipment operation sequences that are currently in failure or have an error. | |
Count of the equipment operation sequences errors or failures. | |
Information about all of the phases in the system. | |
List of all phases currently in failure or have an error. | |
Count of the phase errors or failures. | |
Information where a batch phase belongs. | |
Phase failure for the specified phase. | |
Name of the specified phase. | |
Last phase message logged into the event journal for the specified phase. | |
All parameters for the specified phase. | |
All parameters for the specified phase including parameter limits and report limits. | |
Pause attribute for the specified phase or equipment operation sequence. | |
Pausing attribute for the specified phase or equipment operation sequence. | |
Status information for the specified phase or equipment operation sequence. | |
Status information for the specified phase or equipment operation sequence including a field for storing automatic pauses at each sequence transition (sequence program) or breakpoint (the PPD Instruction in a phase program). | |
Request value for the specified phase. | |
Single-step flag for the specified phase or equipment operation sequence. | |
State of the specified phase or equipment operation sequence. | |
Returns the current step index for the specified phase. | |
Current unit for the specified phase or equipment operation sequence. | |
List of all phases, corresponding equipment IDs, and valid units. | |
List of all equipment phases, corresponding equipment IDs, recipe phases, the phase type and valid units. | |
List of all equipment phases, corresponding equipment IDs, recipe phases, phase types, bitmap files, and valid units. | |
Graphical data for an SFC. | |
Graphical data for an SFC, including transition names and comment information. | |
Graphical data for an SFC, including transition names and comment information. This item supports parameter and report expressions. | |
Recipe report parameters for a procedure. | |
Status data for an SFC. | |
Status data for an SFC to support showing the status of report and parameter expressions. | |
Set of unit requirements configured within the specified recipe structure. | |
Bitmap index for all process cells within the system. | |
Information about all units in a process cell. | |
List of process cells in the current area. | |
List of process cells in the current area, including the process cell class name. | |
Path to the recipe directory. | |
Recipe information for all recipes released to production. | |
Tag status information for all tags associated with the phase and state machine information to indicate the current status of the phase. | |
Tab-delimited list of hyperlinks configured in the area model for the equipment element identified by the resource ID. | |
Resource name denoted by the resource ID. | |
List of all resources and corresponding IDs currently owned by the operator. | |
List of all resource owners and the corresponding owner IDs. | |
List of all resources requested by the operator. | |
List of all resource requesters and the corresponding owner IDs. | |
List of the cross invocation strings associated with the resource specified by the resource ID. | |
List of all resources and corresponding equipment IDs. | |
An XML list of all resources and corresponding equipment IDs. Recommended for use with large resource lists. | |
Indicator of whether the server is running in demo or production mode. | |
Time stamp when the Material Server started. | |
Information for individual signature requests, excluding those generated by private interfaces. | |
List of all outstanding signature requests, excluding those generated by private interfaces. | |
Time stamp of when the FactoryTalk Batch Server started. | |
List of all dynamic owners (control recipes) and owner IDs. | |
Labels used for the generic strings. | |
Internationalized string indicating the current state of the tag verification process. | |
Returns an integer indicating the current state of the tag verification process. | |
Thousands separator used by the FactoryTalk Batch Server as read from the Control Panel . | |
Current time from the FactoryTalk Batch Server and the conversation status of the data servers. | |
Current time from the FactoryTalk Batch Server and the most severe conversation status of all defined data servers. | |
Retrieves information about the selected static information for a timer step on the batch list. | |
Retrieves dynamic information about a specific timer step. | |
Retrieves retrieves selected information about all of the timer steps currently on the batch list. | |
Total number of tags, phases, and equipment operation sequences configured in the equipment database. | |
Unacknowledged prompt area. | |
Unacknowledged prompt batch ID. | |
Default value for the x th unacknowledged event in the unacknowledged event list. | |
Unacknowledged prompt description. | |
Unacknowledged prompt engineering units. | |
Unacknowledged prompt event type. | |
Unacknowledged prompt event ID. | |
Unacknowledged prompt high. | |
Unacknowledged prompt low. | |
Unacknowledged prompt phase. | |
Unacknowledged prompt process cell. | |
Unacknowledged prompt recipe. | |
Unacknowledged prompt response type. | |
Unacknowledged prompt time. | |
Unacknowledged prompt unit. | |
Unacknowledged prompt value. | |
List of unacknowledged prompts. | |
Unacknowledged prompt count. | |
Bitmap index for all units. | |
Operator entered batch ID for a batch running in the specified unit. | |
List of all the equipment operation sequences within the specified unit. | |
List of filenames for the bitmaps within the unit. | |
List of all the phases within the specified unit. | |
List of all the phases within the specified unit, including whether there is an associated control strategy. | |
Unit name, unit class, and tag status information for the specified unit. | |
Set of binding preferences configured on the specified unit requirement. | |
Set of binding requirements configured on the specified unit requirement. | |
List of all units, corresponding equipment IDs, and unit classes. | |
Total number of verified tags, phases, and equipment operation sequences. This total includes tags, phases, and equipment operation sequences that were successfully verified and those that failed verification. | |
Server software version. | |
Most recent warning message in the FactoryTalk Batch Server log file. |
Provide Feedback