ListSeparator

The
ListSeparator
item returns the list separator used by the
FactoryTalk Batch
Server.
This table shows the input and output formats for this item.
Input Format
Request:
ListSeparator
Output Format
The ListSeparator item returns in this format:
<Separator>
Field Name
Format
Descriptio
n
<Separator>
ASCII – String
Default list separator for the language-specific operating system.
This table shows an example of the return on this request.
Example:
A request on
object.GetItem(ListSeparator)
could return:
,
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal